Back

Bids&Projects SCADA and Security rail sector

Job Description

Siemens Mobility is a separately managed company of Siemens. As a leader in transport solutions for more than 160 years, Siemens Mobility is constantly innovating its portfolio in its core areas of rolling stock, rail automation and electrification, turnkey systems, intelligent traffic systems as well as related services. With digitalization, Siemens Mobility is enabling mobility operators worldwide to make infrastructure intelligent, increase value sustainably over the entire lifecycle, enhance passenger experience and guarantee availability. In fiscal year 2019, which ended on September 30, 2019, the former Siemens Mobility Division posted revenue of €8.9 billion and had around 36,800 employees worldwide.


We wanto to join a professional in Bids and Projects SCADA & Security rail area: 

• Main tasks to be performed by the Bids and Projects SCADA & Security Engineer:

o Performs the analysis of tenders and bids specifications provided by customers in the context of Rail Communications and Digital Station projects.
o Develops Bid Technical Specifications and related activities needed for the bid work.
o In the context of Digital Station projects, defines the System Technical Specifications, the System Architecture Specifications and the integration with third-party systems ( Railway Signaling, Communication Networks, end-devices, etc ) developing the Interface Specifications at HW and SW level. 
o Performs the analysis, management and traceability of the SCADA / communication system and Digital Station requirements during the bid and/or project phase. 
o Supports Siemens procurement team in technical clarifications /negotiations with partners / suppliers/third parties, being the technical representative of the SCADA/communication system or subsystem.
o Produces optimal Bill of Material and material dimensioning for Rail Communications and Digital Station Projects.
o Is able to liaise effectively with other engineering teams.
o If required, supports the hand-over of bids technical assets (scope, specifications, requirements…) to the engineering groups during the project phase.

• It is a profile of a horizontal nature, where demonstrable technical skills and expertise in several of the following technologies and areas of knowledge would be valuable:
o SCADA and Control Systems. Proven experience in programming and deploying PLC’s systems for railway environments.  
o Fixed and Radio Communication Networks used in transportation systems: Gigabit Ethernet, SDH, MPLS, IEEE 802.11 based, etc.
o Voice communication Systems
o Passenger Information Systems 
o CCTV / Access Control/Intrusion detection

• It is important also to have:

o Good availability for travelling.
o Good English skills, both spoken and written.
o Good command for the project technical documentation.
o Good communicating and integrating skills, both oral and written. The systems object of the activity in this position are developed in the context of large railway infrastructures, international and heterogeneous environments, both from human and technical perspectives. 

Siemens aboga por la igualdad de oportunidades entre mujeres y hombres, así como en la Diversidad como fuente de creatividad e innovación. Contar con diferentes tipos de talento y de experiencias nos hace ser más competitivos y estar mejor preparados para responder con éxito a las demandas de la Sociedad. Por ello, valoramos a las candidatas y a los candidatos que reflejen la Diversidad que disfrutamos en nuestra Compañía y animamos la cobertura de puestos por mujeres y hombres en ocupaciones que se encuentren subrepresentadas.

Organization: Siemens Mobility

Company: Siemens Rail Automation S.A.U.

Experience Level: Mid-level Professional

Job Type: Full-time

Can't find what you are looking for?

Let's stay connected

Can't find what you are looking for?